Export Archive Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

Menu Selection: Item > Export Item

In the BCT, exports the selected item and its child objects displayed beneath it in the navigation tree in the source selection. The items can be imported into another archive database, see the Import Wizard section for more information.

Procedure

  1. Select the item in the navigation tree in the Source selection.
  2. In the File Name selection, add a new file name or select an existing file name for the file you are exporting and check the Overwrite check box.
    Figure 1. Export Archive Wizard

    The exported data file is stored in the following default directory:

    • C:\ProgramData\Johnson Controls\BCMIII\DatabaseFiles

    Click the Details button for a Notice Information dialog box which displays the Reference, Class, Class Version, Parent Exists and Objects Exists information.
  3. In the Summary Selection click Finish to confirm the export configuration information.