Wizards - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Wizards make complex tasks easy and guide you through creating and configuring objects and features. A wizard typically consists of a series of steps, each corresponding to a screen presented to the user.

A wizard may appear when you select an option from the Insert menu and when you prompt certain actions such as copying and pasting an item in the Navigation Tree. For example, a wizard appears when you select Object from the Insert menu. Wizards that are available in different modes (for example, any combination of online, offline, or simulation) appear the same.