Printing the Entire Help System - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

The entire Help system is available for printing in Adobe PDF format.

To print the entire Help system:

Procedure

  1. If necessary, download Adobe ReaderĀ® (required to view the PDF file) from the Adobe Reader site.
  2. Go to the QuickLIT Product Information Web site or insert the QuickLIT CD.
  3. In the tree on the left, browse to BCPro system > General System Information.
  4. On the right side of the window, click BCPro system Help. The Help PDF opens in Adobe Reader.
  5. On the File menu of Adobe Reader, select Print.

Results

Note: This file is large (over 250 pages). Allow plenty of time for downloading and printing.