Time Sync Period - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Specifies the interval at which the Site Director polls the defined STS (for example, the Atomic clock) for the time. We recommend leaving the default value for this attribute. This attribute applies only to the BCPro Workstation. The time zone is set through the Windows operating system on BCPro Workstation computers.

Back to Site Attributes.