Poll Rate - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Specifies the frequency at which the Site Director checks its communication status with site devices. This setting affects the detection time of offline devices, and the amount of network bandwidth needed to support this detection. At the default setting Fast, the detection time is short, but the network bandwidth use is high. At a Slow setting, the detection time is longer, but network bandwidth use is low. The calculated Detection Interval is shown in the NxE.

Back to Site Attributes.