This attribute is used only for Windows time synchronization. Leave this attribute blank if you are not using Windows time synchronization. Specifies a list of resolvable host names or IP addresses of SNTP server devices that the devices on the site (except the Site Director) use as their time server. Periodically, each device on the site (except the Site Director) attempts to synch time from an SNTP server from this list. Contact with an SNTP server is attempted one at a time in list order until one successful contact is made. A host name may be specified only if a DNS server is available to the site server. If the site server is also an SNTP time server, the site server may be specified in this attribute. This attribute is distributed automatically to the site devices.
Back to Site Attributes.