Site Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Site Object Attributes - Site View Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

All Items Update In Progress

True or False

CW

False

 

Device Time Servers

List of value sets

CW

   

Poll Rate

One type from a set

CW

Fast

Fast, Medium, Slow

Site Director

Set of values

CW

0.0.0.0

 

Site Time Servers

List of value sets

CW

   

Time Sync Period

Number

CW

   

Time Zone

One zone from a set

CW

Central Time

(US and Canada)

Uses Time Zone (Set 576).

Note: The changes made to labels on Object Categories in the Site Object are shown in the Security Administrator screens. Refer to the Object Category Assignment section of the Security Administrator System Technical Bulletin (LIT-1201528) for more information on changing Object Categories labels and how these changes affect the UI.
1 C - Configurable, W - Writable