Average Output Computation - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

In the case of binary types of input references, if the majority of inputs are at State 1 or the inputs are evenly split between State 1 and State 0, the Average output is commanded to State 1. If the majority of inputs are at State 0, the Average output is commanded to State 0.