High OR - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Specifies the object attribute whose value is updated using the highest input of all the inputs in the Signal Select object, for analog point types. For binary point types, the value is updated using a logical OR condition of all inputs of the Signal Select object.

Back to Signal Select Attributes.