Signal Select Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Signal Select Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Average Output

Attribute reference

CNW

None

 

Execution Priority

One state from a set

CW

Normal

 

Failsoft

Real Value

CW

   

High OR

Attribute reference

CNW

None

 

Input List

List of attribute references

CW

 

Minimum number of elements in the list =1,

Maximum number of elements in the list = 12

Low AND

Attribute reference

CNW

None

 

Point Type

One type from a set

CW

Analog

Analog or Binary

Present Value

One value from a set

C

Master

N = 3

0 = Calculated, 1 = Last Reliable, 2 = Fail Soft

Reliability

One state from a set

   

Reliable or Input Unreliable

Setup

One state from a set

C

Last Reliable

n = 2

0 = Last Reliable, 1 = Fail Soft

1 C - Configurable, N - Value Not Required, W - Writable