Signal Select Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Signal Select object can process values from multiple zones to adjust various setpoints and can function with either analog or binary points.

For analog point types, the Signal Select object determines (one or more of) the low input, average input, and/or high input values for use in updating an attribute value of another object.

For binary point types, the Signal Select object determines (one or more of) the average state, the logical Or state, and/or the logical And state values for use in updating an attribute value of another object.

Computations take place at startup and at each time an input value experiences a change in value or reliability. The results of these calculations are sent to specified output points as commands. For example, this object allows you to average multiple zone temperatures and base a control, such as adjusting a setpoint, on that average.

For general information on BCPro system objects, see the Object Help section.