Security Copy Considerations - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
When using the Security Copy Wizard, keep the following considerations in mind:
  • If you want to restore a supervisory device or workstation security database in an BCT, you must use the Security Copy Wizard.
  • If an BCT and BCPro Workstation reside on the same computer, the security database is shared between them both and can be restored using the Security Copy Wizard.
  • If a BCT is not installed on a BCPro Workstation, you cannot use the Security Copy Wizard to restore the BCT security database.