Security Copy - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Two types of database load wizards exist:
  • the Manage Archive Wizard for uploading, downloading, and synchronizing archive (configuration) databases
  • the Security Copy Wizard for restoring the Security System databases of the BCPro Workstation, Router, and Gateway devices

Both wizards use the ActionQueue (ActionQ) to initiate and monitor the load or restore process. The Security Copy Wizard is described in this section. For information on the Load Wizard, see Database Uploading, Downloading, Upgrading Device and Synchronization.

Use the Security Copy Wizard to restore security system databases of the BCPro Workstation, Router, and Gateway devices. The BCT archive database stores the security system database information.

Access this wizard by selecting Security Copy from the Tools Menu in the BCT (offline mode). The Security Copy Wizard collects information necessary to perform the security database restore such as action type, device names, and scheduled time. Once you complete the wizard, the restore commands are added to the ActionQ in the BCT. The ActionQ initiates and monitors the process.

For more information on the ActionQ, see ActionQ.

For information on uploading, downloading, and synchronizing archive databases, see Database Uploading, Downloading, Upgrading Device and Synchronization.