Scheduling the Enabled Audit Level - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

To schedule the Enabled Audit Level based on time using the Scheduling feature:

Procedure

  1. Create a Schedule or display the desired Schedule.
  2. In the Scheduled Items tab, add the desired BCPro Workstation, Router, or Gateway and select the Enabled Audit Level attribute. Follow the steps in the Adding Scheduled Items procedure.
  3. On the Weekly Schedule tab, configure the events as desired. Follow the steps in the Adding Weekly Scheduled Events and Editing Scheduled Events procedures to schedule specific days and times to change the Enabled Audit Level. See the Workstation Device Object’s Enabled Audit Level attribute description for information on the levels you want to schedule.
  4. Click Save.