Creating a Schedule or Calendar - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

Note: The procedure for creating a schedule or a calendar in offline mode (using BCT) is the same as the online procedure using the Insert Object Wizard. See BCPro Data Server Modes for more information about the modes of operation.
Note: You cannot create schedules or calendars in an FAC from BCT or BCPro.

Procedure

  1. From the Insert menu, select Object. The Insert Object Wizard appears.
  2. Select Schedule or Calendar and follow the Insert Object Wizard instructions.
    Note: Add extensions to the schedule or calendar at the wizard prompt, if desired. See Extensions.