Copying and Pasting a Schedule or Calendar (Offline Mode Only) - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

Note: This procedure is available only in offline mode (BCT).
Note: This function is not available for schedules/calendars in an FAC.

Procedure

  1. In offline mode, select the schedule or calendar from the navigation tree.
  2. Select Copy from the Edit menu.
  3. Select the desired destination for the copied schedule or calendar in the navigation tree.
  4. Select Paste from the Edit menu. The Paste Object Wizard appears.
  5. Edit the name of the schedule or calendar as desired and click Paste.