Adding Scheduled Items - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Procedure

  1. Display a Schedule.
  2. From the Display Mode drop-down menu, select Scheduled Items.
  3. Click Edit.
  4. Click the add (green plus) button.
  5. Select one or more items from the Select Item dialog box and click OK.
    Note: To select multiple items, use the Control or Shift key.
  6. The system automatically chooses the default attribute for each item you selected. To choose a different attribute, click the ellipses icon button and select the attribute that you want to schedule.
  7. Click Save.
    Note: The first item in the list of scheduled items (Table of Scheduled Items) determines the data type used when the schedule writes values to the attributes of the scheduled item.