Weekly Schedule - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The scheduling feature has a weekly schedule that provides a schedule for each day of the week, Monday through Sunday. Each daily schedule begins at 00:00 and ends at midnight (the display reads 23:59). Each day consists of events that initiate the writing of values to the referenced attributes of the scheduled items based on the day of the week. For example, you can schedule a fan to start at 7:00 and stop at 22:00 on Mondays.

To edit the weekly schedule, double click or right-click on the weekly schedule. Right-click brings up the context menu (see Table 2).