Effective Period - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The effective period defines the active or inactive date range for a schedule (weekly and exception schedule). In Edit mode, the ellipses icon button opens the Effective Period dialog box. By default, a schedule is always active.

For example, you can create two schedules with the same items/objects and configure one for the heating season and the other for the cooling season. Then you can define the effective period of the heating schedule from October through March and the cooling schedule from April through September of each year.