Global Calendar - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

The Global Calendar allows you to make facility-wide changes to calendars, such as defining holidays. These changes are tedious if you need to edit many calendars. To solve this problem, you can reference a Global Calendar object in each FAC or supervisory device. When you edit the values of the Global Calendar object, the dates automatically download into all the local calendars.

To reference a Global Calendar object:

Procedure

  1. To create a calendar object - in the Configuration tab, click to choose the Global Calendar Object Reference.
    Figure 1. Global Calendar Object Reference - Configuration Tab
  2. To edit attributes of a calendar - in the Advanced Focus tab, click Edit and click the ellipses icon button to choose the Global Calendar Object Reference.
  3. Click Save and the Configuration tab will add the date and time of the last Global Calendar Update.
    Figure 2. Global Calendar Update