Enable - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Enable command allows the Schedule object to resume normal scheduling operation. The Schedule object starts the schedule as soon as it is enabled. When it is re-enabled, the Schedule object writes its current value to the scheduled items.