Disable - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Disable command stops all future scheduled events. Neither the Weekly Schedule nor the Exception Schedule run again until the Schedule object is re-enabled. While disabled, the status log in the Scheduled Items view lists the object as disabled. The schedule remains disabled until re-enabled.