Status Flags - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
The Status Flags indicate the general health of the object. This attribute does not appear in the BCT.
Table 1. Status Flag Descriptions

Status Flag

Description

In Alarm

This flag is always False for the Schedule object.

Fault

False means that the Reliability attribute is reliable, otherwise the flag is True.

Overridden

This flag is always False for the Schedule object.

Out of Service

True means that the Out of Service attribute is also True, otherwise the flag is False.