Description - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Description attribute contains a user-defined description of the object. The Description attribute allows up to 40 characters, but is not required. Description is a common object attribute; for more information, see Common Object Attributes.