The Priority for Writing attribute defines the priority at which the referenced attributes are commanded. Seven is the highest priority and 16 is the lowest supported by the Schedule object, with the default of 15.
Note: We do not recommend using priorities 7 or 8 as they may interfere with the operator override functionality.