Schedule Output Type - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
The Schedule Output Type attribute indicates the value type of the Schedule object’s Present Value, Default Schedule Command, and all scheduled events.
Table 1. Schedule Output Type Options

Option

Description

Binary

Select this option to set the schedule’s Value type to Binary (one of two states, such as Off and On).

Analog

Select this option to set the schedule’s Value type to Analog (for example, 72.0).

Multistate

Select this option to set the schedule’s Value type to Multistate (one of a set of states, such as Off, Low, Medium, and High).

Derived from Key Item

Select this option to set the schedule’s Value type to match the Value type of the attribute scheduled for the Key Item. For example, all values are Boolean (True/False) if the Key Item’s Enabled attribute is scheduled.

Derived from Value

This type is only set by the system - it cannot be manually selected. This type indicates that the current schedule type matches preexisting values.