Effective Period - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Effective Period attribute defines the range of dates within which the Schedule object is active. By default, these dates are unspecified, causing the Schedule object to be active for all days. When the Schedule is not within the Effective Period, the Schedule is considered Inactive and the Schedule’s status is set to Inactive. Wildcards may be used in the date fields. For more information on using wildcards, see Wildcards.