Weekly Schedule - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains a timeline of events for each day of the week - Monday, Tuesday, . . . Sunday. Each event has a time and value that the Schedule writes to the scheduled objects. An event ends at midnight, but it can be ended earlier by specifying an end time or by scheduling another event to start. Events in the Exception Schedule override times and values in this Weekly Schedule. If the Weekly Schedule has no events defined on a particular day and time, and there are also no exception events scheduled, the Default Schedule Command takes effect.

Note: Weekly Schedule does not display for third-party schedules that do not support a weekly schedule.