Today's Schedule - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains the schedule timeline for the current day. The timeline displays the projected schedule output that will be written to the scheduled objects for the current day, combining the default Schedule Command with events from both the Weekly Schedule and Exception Schedule. Today’s Schedule also displays a table of times and values, which details the changes in the schedule’s output for the current day.

Note: Today’s Schedule does not display in the BCT. It also does not display for mapped third-party schedules.