Contains the list of items to be commanded by the schedule object. If empty, the Schedule does not directly command objects but its Present Value can still be used as an input to other logic, such as an Interlock or Control System. The online display also includes a Status Log that shows the status of the schedule’s attempts to control each of the scheduled items. If no objects are scheduled, the Schedule Output Type determines what type of command may be scheduled.