Schedule Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Schedule object works behind the scenes of the Scheduling feature. The Schedule object updates attribute values of objects according to the time of day. These times can be specified for days of the week and as exceptions.

For more information on the Scheduling feature or the steps it takes to create one, see the Scheduling section.

For general information on BCPro system objects, see the Object Help section.