Database - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The database is the collection of objects and their parameters as defined by the user. Each database is unique to the job. A database can be created or edited (with appropriate user authority) either online using the Building Manager Portal UI, or offline using the Building Configuration Tool (BCT). BCT can also be used to download a database or upload and create a backup copy of the database.