Object Identifier - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the instance number of the Object Type used in the BACnet Object ID as exposed to a BACnet network. The object ID must be unique within the host device. The object ID of the Device object must be unique within the BACnet network.

Back to Router Attributes.