Max Master - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Specifies the highest possible address for master nodes and is less than or equal to 127. This is present if the device is a master node on an MS/TP network. If Max Master is not writable via BACnet services, its value is 127.

Back to Router Attributes.