Represents the IP address of one or more default gateways. A write to this attribute is ignored when the DHCP Enabled attribute is True. A read of this attribute returns either the user specified value or the value determined from DHCP. Certain IP router addresses are invalid and cannot be written successfully. See the description of the IP Address.
The IP Router Address attribute may be set explicitly, or it may be automatically set using the DHCP server. Using a DHCP server may change this attribute even if you have set it up explicitly. See the DHCP Enabled attribute.
Back to Router Attributes.