BACnet Integrated Objects - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
  • Include in Object List - Makes internal integration objects visible to BACnet devices. This is the default value.

  • Exclude from Object List - Makes internal integration objects unavailable to BACnet devices.

When this attribute is set to Include in Object List and Routing Mode is set to Enabled, the same third-party object appears in the list twice (as a native object on the actual device and as an integrated object within the Router); therefore, this setup is not recommended. When Routing Mode is set to Enabled Without Broadcasts, it prevents third-party devices outside the network from discovering devices on a routed network using broadcast data.

Back to Router Attributes.