Indicates the maximum number of times that an APDU (as specified by the BACnet device) is retransmitted. If the device does not perform retries, it is set to zero. If the value is greater than zero, a nonzero value appears in the APDU Timeout attribute.
If you write the value of this attribute, you must restart the Router for the new settings to take effect.
Back to Router Attributes.