Router Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab and the Diagnostics tab.

Click the attribute name in the table for a description of the attribute.

Table 1. Router Device Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Flags 1

Initial Value

Values/Options/Range1

APDU Retries 2

Number

CW

4

2–10

APDU Segment Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

APDU Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

Archive Date

Date

     
BACnet IP Port 2

Number

CW

47,808

0–65,535

Baud Rate Selection

One state/type/mode from a set

   

0 - 4194303

BIOS Version

Text

     
Device Object Identifier

Number

C

B

Instance Number of Object Type within the host device.

DHCP Enabled

True or False

CW

True (1)

0 = DHCP disabled,

1 = DHCP enabled

Firmware Version

Text

     
Local Date

Date

     
Local Time

Time

     
MAC Address

Number

C

 

0-255

Max Info Frames

Number

   

10 (FEC)

100 (Router)

Max Master

Number

   

127

Max Segments Accepted

Number

     
Model Name

Text

 

CN-BRTR-0

 
Network Address 2

Number

CW

1,001

0–65,535

Power Consecutive Samples

Number

CW

5

0–32

Power Sampling Interval

Number

CW

1

0–32

Units = Seconds

Remote Network Address

Number

   

1-65,534

Table 2. Router Device Object Attributes - Diagnostic Tab

Attribute Name

Data Type

Flags 3

Initial Value

Values/Options/Range3

Active Baud Rate

One state/type/mode from a set

C

 

Use 38400 baud only. This value is the recommended baud rate for bus supervisor ports.

BACnet Routed Messages Rate

Number

   

Units = Per Minute

Battery Charging

True or False

   

This attribute appears in only the BACnet Router and Modbus Gateway.

Battery Condition

One from a list of conditions

   

Uses Ok Fault (Set 161) or Battery Condition (Set 175).

Board Temperature

Real value

   

Units = Deg C

Display Precision = 1

COV Increment = 1.0

Memory Usage

Number

   

Units = %

Display Precision = 0.01

COV Increment = 0.1

Token Loop Time

Number

   

0–4,294,967,295

Milliseconds

Table 3. Router Device Object Attributes - Network Tab

Attribute Name

Data Type

Flags 4

Initial Value

Values/Options/Range 5

BACnet Integrated Objects

One from a list of objects

C

   
Computer Name 6

Text

W

 

See attribute description.

DHCP Enabled

True or False

CW

True (1)

0 = DHCP disabled

1 = DHCP enabled

DNS Server IP Addresses

List of numbers

CW

 

List of IP addresses.

Domain Name 6

Text

W

   
Ethernet MAC Address

List of numbers

     
IP Address

List of numbers

CW

 

Any valid IP address

IP Mask

List of numbers

CW

   
IP Router Address

List of numbers

CW

   
Obtain DNS Address Automatically

True or False

CW

True (1)

 
Routing Mode

One from a list of values

CW

   
1 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
2 If you write the value of this attribute, you must restart the Router for the new settings to take effect.
3 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
4 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
5 If you write the value of this attribute, you must reset the Router for the new settings to take effect.
6 If you change the value of this attribute, the Router automatically resets.