Router Device Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

The Router object defines the attributes that represent the externally visible characteristics of the BACnet Router of the BCPro system. One Router Device object exists per BACnet Router.

Note: The Object Type for this object is labeled Device in the software.

This object allows you to see data about the router, such as the IP address and the current date and time.

For general information on BCPro system objects, see the Object Help section.