Summary Tab - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Summary tab provides summary data for items in the navigation tree. For example, the Summary tab of the MSTP Field Bus object shows summary data for the devices on the field bus. The Summary tab shows the status, icon, item, value, and description information of the items. You can view and edit items on this tab using the right-click menu options.

Note: Data appears in the Status column of the Summary tab when the status is not Normal (for example, High Alarm).