Options Tab - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Attributes associated with the default state, control source, and restart options for an object are shown under the Options tab of the display panel.

Table 1. Options Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Auto Restore

True or False

CW

True

Applies to AO, BO, and MO objects.

Ignore Relinquish Default

True or False

CW

True

Applies to AO, BO, MC, and MO objects.

Local Control

True or False

CW

True

Applies to AO, BO, and MO objects.

Relinquish Default

Real value

CW

 

Range = Min Value - Max Value

Applies to AO, BO, MC, MO, AV, BV, and MV objects.

Restore Command Priority

Set of values

CW

Operator Override

Uses Restore Priority (Set 357).

Applies to AO, BO, MC, MO, AV, BV, and MV objects.

1 C - Configurable, W - Writable