Displays the Instance Number of the object on the remote field device. The Instance number, along with the object type, defines the remote object’s BACnet Object Identifier. The BACnet Object Identifier is used to establish communication with the object.
Back to MS/TP Hardware Tab.