Indicates the baud rate of the device's FC bus (Table 1).
|
Baud Rate |
Description |
|---|---|
|
Auto |
Use baud rate of running network. This value is the recommended setting for everything on the FC bus except the bus supervisor port. See Active Baud Rate. |
|
1200 |
Use 1200 baud only. This value is not recommended and may not be allowed on some devices. |
|
9600 |
Use 9600 baud only. This value is the lowest standard MS/TP baud rate. |
|
19200 |
Use 19200 baud only. This value is not recommended. |
|
38400 |
Use 38400 baud only. This value is the recommended baud rate for bus supervisor ports. |
|
76800 |
Use 76800 baud only. |
Back to MS/TP Hardware Tab.