Instance Number - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains the number of mapped BACnet objects that are being polled on a periodic basis or are part of the BACnet Object Identifier (along with the Object Type). The BACnet Object Identifier is used to establish communication with the object.

Back to BACnet Hardware Tab.