Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. These attributes are not exposed to a BACnet network.
Note: Each Hardware attribute table is organized and divided into sections of Integration Hardware attributes, Device Hardware attributes, and Point Hardware attributes (calling out when attributes are shared between these object types). These sections are indicated by headings that span across the table.
|
Attribute Name |
Data Type |
Notes 1 |
Initial Value |
Values/Options/Range |
|---|---|---|---|---|
|
BACnet Device Hardware Attributes |
||||
|
True or False |
CW |
False |
False True |
|
|
BACnet Device and Point Hardware Attributes |
||||
|
Number |
C |
None |
0–65,535 |
|
|
Series of numbers |
None |
BACnet device address |
||
|
Text |
None |
|||
1 C - Configurable, W - Writable