Focus Tab - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Focus tab appears when you define an object in the online Site Management Portal. The Focus tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Focus tab varies by object type. For example, the Analog Input object’s Focus tab has different attributes than the BCPro Workstation object’s Focus tab. See the specific object section for details on its Focus tab.

Note: This tab is called the Configuration tab in the BCT or in a Wizard.