Diagnostic Tab - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Diagnostic tab only appears for objects containing diagnostic data. The attributes displayed on the Diagnostic tab vary by object type. For example, the Diagnostic tab of the BACnet Protocol Engine Object has different attributes than the BACnet Integration Object. See the specific object section for details on its Diagnostic tab. Also, see the Diagnostics section.