Configuration Tab - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Configuration tab appears when you define an object in the BCT or in a Wizard. The Configuration tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Configuration tab vary by object type. For example, the Analog Input object’s Configuration tab has different attributes than the BCPro Workstation object’s Configuration tab. See the specific object section for details on its Configuration tab.

Note: This tab is called the Focus tab in the online BCPro system.