State, Mode, and Type Sets - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

State, Mode, and Type Sets provide the source of readable text for the user interface when the displayed value can be one of many states, modes, or types. For example, the Status attribute of every object is displayed as one of the texts listed in the Object Status (Set 505).

References to specific sets appear throughout the Object Help, usually in the Values/Options/Range column of the object’s attribute table.