Object Naming Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Every object can be identified by one of three naming attributes.

Name - a freely definable user name for the object

Item Reference - a fixed name used internally by the system

BACnet Object Name - the name exposed to a BACnet network based on the Item Reference.

See the Object and Feature Tabs section for more information on these attributes.